Filtrovat podle
Nalezen výsledek pro CMM
Renishaw and Status Metrology Official Channel Partnership sets new standards for service delivery
Renishaw and Status Metrology have enjoyed a trusted customer supplier relationship.
TP20 modules
TP20 stylus modules
UCC daughtercards (H-1000-5220)
There is a range of UCC daughtercards available each card offering additional capabilities to the standard UCC1 or UCC2 product.
MSL using Renishaw's PH20 5-axis touch-trigger system (image courtesy of MSL)
Renishaw, one of the world’s leading precision engineering and scientific technology companies, has announced the appointment of Measurement Solutions Ltd (MSL) - the Peterborough, UK-based scanning...
FCR25 change rack (triple-port unit for MRS system)
The FCR25 flexible change rack is a triple port unit that has been designed to provide unmatched flexibility where rapid automatic changing is required.
Tower Malacky - Flexible consistent inspection at Porsche part supplier
Tower Malacky, the Slovakian subsidiary of US company Tower, is a leading supplier of pressed parts to blue-chip motor manufacturers across Europe, such as Porsche and Volkswagen.
PEM3 200 mm extension bar
PEM multiwired extension bars, available in three lengths, extend the reach of autojointed probes.
MH20 and MH20i fault finding
MH20 and MH20i fault finding TP20 module Poor measuring performance: Possible cause Remedy Stylus configuration too long or not rigid.
Automatic operation
Automatic operation ACR2 port datuming procedure: Change cycles To change probe arms automatically using the ACR2, the CMM must be programmed to complete a series of movements using...
Calibration and capability artefacts for SFP2 surface finish probe (H-1000-2500)
Surface finish measurement has traditionally involved the use of hand-held sensors or has required the part to be moved onto a costly dedicated measuring machine.
MH20 and MH20i (H-1000-5195)
The MH20 and MH20i are manually operated probe heads that articulate to provide orientation of the probing axis.
Improved measurement performance with new motorised heads for co-ordinate measuring machines
Following a series of design enhancements, Renishaw’s industry-standard family of PH10 motorised indexing heads for co-ordinate measuring machines (CMMs) now have a 20% improvement in repeatability...
UK manufacturing switches on to REVO®
Renishaw is delighted with the response to the first REVO seminars, held in September and attended by engineers from automotive, aerospace and subcontract manufacturing.
UK Automotive Open House 2017 during a CMM products demonstration
Global engineering technologies company Renishaw hosted a UK Automotive Open House on Thursday 6th April, where leading manufacturers from all over the UK heard how Renishaw could improve their...
New MODUS™ CMM software supports powerful 5-axis measurement
Powerful new metrology softwar
New MODUS™ CMM software supports powerful 5-axis measurement
Powerful new metrology softwar
Autochange software
Autochange software Responses from ACC2-3 Responses from the ACC2-3 fall into three categories: Normal status messages Error state messages Rack status messages These responses are...
MIH installation
MIH installation Fitting the battery Move MIH to axis positions A0.
ACR2 autochange rack
ACR2 autochange rack Extension arm changing system for the PHS-2 servo positioning head system Enables probe head extensions (HE) or probe head adaptors (HA) to be exchanged to suit the probing...
Reference marks
Reference marks Probe orientation with reference marks nominally at zero: Axis rotational alignment Rotational alignment of the head axes can be found by using the spirit level tool (part number...
Lifting
Lifting This denotes the lifting points on the cabinet: WARNING: Specified cabinet weight is 65 kg with no control equipment installed.
MIH
MIH The MIH features an autojoint probe mount for fast, repeatable probe changing.
SPA3-2 600 W PSU installation
SPA3-2 600 W PSU installation WARNING: Output terminal cover must be re-fitted after termination.
FCR25
FCR25 Extended warranty For peace of mind a 3-year warranty is available for your new CMM products during the first 3 months from purchase.
ZH-TW - 安全
ZH-TW - 安全 行走移動零件之間以及行走移動零件與靜止零件之間存在夾傷的危險。 在移動時或手工更動換測頭時,切勿握住測頭座。 謹防意外移動。 使用者位置應保持在測頭座/延長桿/測頭組合件的整個工作包覆面以外。 在使用工具機或 CMM 的應用程序中,建議採用眼部防護措施。 某些裝置設有外接空氣管。 務必謹慎確保空氣管安全固定於倒鉤型氣動接頭。 有關 Renishaw 公司產品的安全清潔...
RO - Instrucţiuni de siguranţă
RO - Instrucţiuni de siguranţă AVERTISMENT: Întreținerea trebuie efectuată numai după ce mașina a fost izolată față de alimentarea electrică, alimentarea cu aer comprimat sau alte surse de...
ES - Seguridad
ES - Seguridad Si aparece este símbolo en el producto, el usuario deberá consultar la guía de instalación para obtener más información y consejos sobre seguridad.
PI 200-3 introduction
PI 200-3 introduction The image below shows the PI 200-3 stand alone version (A-5707-0100): The image below shows the PI 200-3 integrated card version (A-5707-0200) that is intended to be used in...
Axis0, Axis1 and Axis2 motor drive connectors (7w2 D socket)
Axis0, Axis1 and Axis2 motor drive connectors (7w2 D socket) Each motor connection is a 7W2 connector for connection of a CMM motor to the SPA3, as shown below: Pin no.
ZH - 安全性
ZH - 安全性 注: PHS-2系统内含有由交流电源供电的装置。 机床制造商有责任确保用户了解操作中存在的任何危险(包括雷尼绍产品说明书中提到的危险),并应确保提供充分的防护装置和安全联锁装置。 在某些情况下,测头信号可能错误地表示测头已就位。 切勿单凭测头信号来停止机器运动。 紧急关闭雷尼绍产品的方法是断开电源。 运动部件之间以及运动部件与静止部件之间存在夹伤危险。 在移动时或手动...
Reference marks
Reference marks Each axis must be referenced to enable its zero position to be set.
PH20 warnings
PH20 warnings Beware of unexpected movement.
IS1-2 safety
IS1-2 safety WARNING: Risk of electric shock – Any interruption in the protective conductor may make the equipment dangerous.
Capital Markets Day - Tuesday 17th June 2025
Capital Markets Day - Tuesday 17th June 2025 Renishaw hosted its 2025 Capital Markets Day for analysts, institutional investors and private shareholders, at its Miskin manufacturing site in Wales on...