Filtrovat podle
Nalezen výsledek pro CMM
Renishaw's Ewan Durie presenting Brian Young with their Channel Partner Programme certificate
Edinburgh-based CMM support and equipment supplier, APEX Metrology Ltd, has been announced as the latest partner of Renishaw’s Channel Partner Programme; the first Scottish company to join the programme.
APEX Metrology Ltd becomes latest Renishaw Channel Partner
Edinburgh-based CMM support and equipment supplier, APEX Metrology Ltd, has been announced as the latest partner of Renishaw’s Channel Partner Programme; the first Scottish company to join the programme.
The Renishaw Equator gauging system in action at APEX Metrology Ltd
Edinburgh-based CMM support and equipment supplier, APEX Metrology Ltd, has been announced as the latest partner of Renishaw’s Channel Partner Programme; the first Scottish company to join the programme.
MODUS™ IP On-machine inspection software
MODUS IP, built on Renishaw’s MODUS metrology software technology, brings CMM-type programming capabilities to the shopfloor.
Automatic operation
Automatic operation Probe calibration: NOTE: Angular orientation of D and E axes required for port datum procedure (D and E 0°).
MCU safety
MCU safety CAUTION: Before unpacking and installing the MCU W system, the user should carefully read the safety instructions below and ensure that they are followed at all times by all operators.
BG - Безопасност
BG - Безопасност ВНИМАНИЕ: Този продукт използва инфрачервени сензорни лъчи.
PH10 compatible probes
PH10 compatible probes M8 touch-trigger probes This range of probes utilises the M8 bush for mounting to the head.
BG - Безопасност
BG - Безопасност Излъчване на инфрачервена светлина LED ПРОДУКТ КЛАС 1 Предупреждения Съществуват рискове от притискане между движещи се части и между движещи се и неподвижни части.
Reporting and analysis
MODUS provides a wide range of text and graphical reports and can output measurement data in a variety of standard formats.
REVO-2 system connections
REVO-2 system connections Installation for 4 - 6 axes with head cable exceeding 25 m and thermal effect compensation (TEC) Key Description Key Description 1 Orange head cable 6 24 V...
PHC10-3 PLUS probe head controller
Dedicated head controller for the PH10 range of motorised heads for use with OEM machine controller systems.
ANT Industries - "There is no other option to REVO, nothing else comes close"
ANT Industries, a supplier to Rolls-Royce, has cut inspection times on complex parts by up to 83%, using Renishaw’s REVO® five-axis measuring system fitted to a Metris CMM.
Manual probe head cable
This straight cable has an in-line 5-pin DIN plug at end 'A' and is unterminated at end 'B'. It electrically connects Renishaw manual probe heads to the CMM quill.
FixtureBuilder Software
FixtureBuilder is a 3D-modelling software package designed to allow the creation and documentation of fixturing set-ups.
RFP1 (H-1000-5430) - legacy
The REVO fringe probe (RFP1) is a non-contact structured light sensor for the REVO® system offering highly accurate measurement of surface topology on an infinite positioning, 5-axis CMM platform.
PI 7-3 (H-1000-7555)
The PI 7-3 is a dedicated signal conditioner for interfacing the TP7M series of probes or touch-trigger probe types such as TP2, TP20 or TP6 / TP6A, to the CMM controller.
RFP1 fringe probe for REVO-2 - legacy
The REVO® fringe probe (RFP1) is a non-contact structured light sensor for the REVO system offering highly accurate measurement of surface topology on an infinite positioning, 5-axis CMM platform.
Manual probe head cable
These coiled cables have a 90° moulded 5-pin DIN plug at end 'A' and an in-line LEMO plug at end 'B'. They electrically connect Renishaw manual probe heads to the CMM quill.
Manual probe head cable
These coiled cables have a 90° moulded 5-pin DIN plug at end 'A' and an in-line LEMO plug at end 'B'. They electrically connect Renishaw manual probe heads to the CMM quill.
Manual probe head cable
This straight cable has an in-line 5-pin DIN socket at end 'A' and an in-line LEMO plug at end 'B'. It electrically connects Renishaw manual probe heads to the CMM quill.
ACR3 autochange rack
ACR3 autochange rack NOTE: Dimensions in mm (in).
PH10 PLUS motorised indexing heads
Family of indexing heads (PH10M PLUS, PH10MQ PLUS and PH10T PLUS) with in-quill and probe mounting options.
Datuming SCP600
Datuming SCP600 NOTE: As the SCP600 port is of modular design, it is suggested that the following routine is completed under manual control for each port installed.
ACR1 warnings
ACR1 warnings Pinch hazards exist between moving parts and between moving and static parts.
Configurable I/O (9W 'D' socket)
Configurable I/O (9W 'D' socket) The connector is a 9W miniature 'D' socket, pinout as follows: Pin number Function Description 1 I/O 0 General purpose input or output 0 2 I/O 1 General purpose...
EL - ΠΡΟΕΙΔΟΠΟΙΗΣΕΙΣ
EL - ΠΡΟΕΙΔΟΠΟΙΗΣΕΙΣ ΣΗΜΕΙΩΣΗ ΑΣΦΑΛΕΙΑΣ Οι θύρες του ACR2 έχουν εξαρτήματα με φόρτιση ελατηρίου που δημιουργούν κίνδυνο συμπίεσης εάν έχουν αφαιρεθεί τα καλύμματα.
IT - AVVERTENZE
IT - AVVERTENZE NOTA DI SICUREZZA Ciascuna porta ACR2 contiene componenti a molla con pericolo di rimanere impigliati se vengono rimosse le coperture.
TP20 introduction
TP20 introduction This installation and user's guide supports the following Renishaw products: TP20 touch-trigger probe system which includes the probe body and probe module (inhibit and non-inhibit...
LT - Sauga
LT - Sauga Įrenginio sauga Kai ant gaminio rodomas šis simbolis, naudotojas privalo informacijos ir saugos rekomendacijų ieškoti įrengimo vadove.
GA - FOLÁIRIMH
GA - FOLÁIRIMH NÓTA SÁBHÁILTEACHTA Tá comhpháirteanna sprionglódáilte i ngach port ACR2 a d'fhéadfadh a bheith ina nguaiseacha cúngúcháin dá mbainfí na cumhdaigh.
PT - AVISOS
PT - AVISOS AVISO DE SEGURANÇA Cada porta ACR2 contém componentes acionados por mola que provocam risco de beliscadura caso as suas coberturas sejam removidas.
UCC T3 safety
UCC T3 safety WARNING: Earthing provision for the complete machine is the responsibility of the OEM or installer.
Support software - UCCsuite
Support software - UCCsuite UCCsuite installation structure The default installation path of UCCsuite puts the files in the following location on the PC hard drive: C:\Program Files...
MH20 and MH20i product description
MH20 and MH20i product description MH20 The MH20 incorporates the TP20 kinematic mount with 2-axis adjustable swivel.
LT - Sauga
LT - Sauga Jei įranga naudojama ne taip, kaip nurodo gamintojas, gali sumažėti įrangos saugumas.
Gauging system accelerates COVID-19 test kit production
In the race to combat the global COVID-19 pandemic, the distribution of coronavirus test kits became a very high priority.
Air system requirements
Air system requirements A clean, dry air supply to the head is required for axis motor cooling to give optimum metrology performance.
Air system requirements
Air system requirements A clean, dry air supply to the head is required for axis motor cooling to give optimum metrology performance.
ACR1 warnings
ACR1 warnings Pinch hazards exist between moving parts and between moving and static parts.
HU - Biztonság
HU - Biztonság FIGYELMEZTETÉS: Az SPA2-2 készüléket le kell földelni.
Ø25 mm datum ball
The Renishaw universal datum sphere is made from hard-wearing tungsten carbide and is supplied with an individual UKAS certificate stating the calibrated ball diameter and roundness.
PBC-1226 - UCClite-2 - support of native interfaces
When we explained our software structure plans in product bulletin PBC-1040 (10th December 2007) and when we announced the launch of the UCClite-2 controller in PBC-1179 (6th March 2008), we implied...