Filtrovat podle
Nalezen výsledek pro CMM
CMM support, training and downloads
CMM support, training and downloads Our knowledgebase library is continually updated with answers to the most frequently asked questions.
UCC T5 PH20 CMM controller installation guide
UCC T5 PH20 CMM controller installation guide Documentation part number: H-1000-7573-07-F For other manuals and product documentation visit www.
CMMs, probes, software and retrofits
CMMs, precision sensors and retrofits offering fast, accurate acquisition of component dimensions and surface data.
CMM cables product compliance
CMM cables product compliance Contact Renishaw plc or visit www.
CMM readhead input connections
CMM readhead input connections Readhead connector (as viewed on the controller rear panel): NOTE: If the machine scale is of a different format (e.
Racks and accessories
Racks and accessories About stylus and probe changing The range of features and components that must be measured in a typical factory means that manufacturers need a flexible measuring solution.
CMM retrofit reduces cycle time by up to 55%
After losing its 3-axis co-ordinate measuring machine (CMM) to a devastating flood, Precision Machine & Auto Components (PMAC) had to act fast to find an alternative solution.
UKCA declarations of conformity - CMM products
UKCA declarations for Renishaw's CMM products.
EU declarations of conformity - CMM products
EU declarations of conformity for Renishaw's CMM products.
Substrate mastered scale on a CMM
The thermal behaviour of an encoder scale is an important consideration when selecting any encoder system.
UCC S5 REVO-2 CMM controller installation guide
UCC S5 REVO-2 CMM controller installation guide Documentation part number: H-1000-7598-04-G NOTE: Please use the left-hand navigation to view this complete document.
Five-axis CMM inspection lets "good times roll"
Scanning probes speed form-data collection and feedback to machining cells, reduce CMM fixturing and cut probe calibration time from hours to minutes at Kawasaki's Maryville, MO plant.
CMM retrofit reduces cycle time by up to 55%
After losing its 3-axis co-ordinate measuring machine (CMM) to a devastating flood, Precision Machine & Auto Components (PMAC) had to act fast to find an alternative solution.
Mounting TCR20 onto the CMM
Mounting TCR20 onto the CMM NOTE: To minimise the machine volume lost it is recommended that the TCR20 is mounted as close as possible to the extreme edge of the CMM's operating envelope.
CMM controller cabinet product compliance
CMM controller cabinet product compliance Contact Renishaw plc or visit www.
R-CPC-190 - CMM plate clamps
R-CPC-190 CMM plate clamps Non-marking clamp for securing 13 mm and 19 mm thick fixture base plates to a CMM.
TONiC™ optical encoders support the latest generation of CMMs from COORD-3
A continuous product development cycle, horizontal organisational structure and streamlined range of model sizes have made COORD-3 a global CMM brand.
Renishaw encoders support the latest in DUKIN’s CMM design
The co-ordinate measuring machine (CMM) has become an indispensable tool in the process control regimes of modern production lines.
Take Messier-Dowty’s lead and actively monitor CMM performance
Do you trust your co-ordinate measuring machines? Take Messier-Dowty's lead and actively monitor CMM performance.
Connecting the UCC2 or UCC2-2 to a CMM
Connecting the UCC2 or UCC2-2 to a CMM The purpose of this chapter is to describe the various connections available within the UCC2 or UCC2-2 design to enable connection to a CMM.
Legacy products
Legacy products For information regarding current products please refer to the 'Installation and user's guide downloads ' page.
Apex improves capabilities and responsiveness through investment in 5-axis CMM technology and flexible gauging
A step-change in macro-economic factors led CMM specialists, Apex Metrology Ltd (Apex), to conduct a strategic review of its service offering.
Alignment of SCP80(V) to the CMM axes
Alignment of SCP80(V) to the CMM axes Alignment of the SCP80 to the CMM axes The alignment of the SCP80 to the CMM axes should be checked to be within the limits shown below.
Alignment of the SCP80(V) to the CMM axes
Alignment of the SCP80(V) to the CMM axes Alignment of the SCP80 to the CMM axes The alignment of the SCP80 to the CMM axes should be checked to be within the limits shown below.
UCC T5
UCC T5 UCC retrofit Renishaw has formed a technical partnership with some of the industry's leading software companies and retrofitters to provide powerful CMM retrofit solutions using Renishaw's...
UCC T3 PLUS and UCC S3 CMM controller installation guide
Powerful 3-axis CMM controller featuring built-in standard touch-trigger and TP200 interface, PH10 PLUS head controller and thermal error compensation (TEC).
Renishaw co-ordinate measuring machine (CMM) technologies at IMTS 2024
Renishaw will demonstrate innovative co-ordinate measuring machine (CMM) solutions for optimised manufacturing at IMTS 2024.
R-PC-13300300-15-8 - M8 CMM Aluminium plate, 12.7 mm × 300.0 mm × 300.0 mm
This CMM precision ground aluminium base plate has multiple M8 threaded holes spaced at 15 mm intervals to increase the flexibility of your fixture.
R-PC-19600600-15-8 - M8 CMM Aluminium plate, 19.1 mm × 600.0 mm × 600.0 mm
This CMM precision ground aluminium base plate has multiple M8 threaded holes spaced at 15 mm intervals to increase the flexibility of your fixture.
R-PC-13450450-15-8 - M8 CMM Aluminium plate, 12.7 mm × 450.0 mm × 450.0 mm
This CMM precision ground aluminium base plate has multiple M8 threaded holes spaced at 15 mm intervals to increase the flexibility of your fixture.
Target points for a manual CMM
Target points for a manual CMM To create Target Points for use on a manual CMM, begin the process by selecting the < Write DMIS sequence.
Renishaw extends its range of AGILITY® 5-axis technology multi-sensor CMMs.
Renishaw, a world-leading manufacturer of engineering and precision measurement systems, now offers a range of co-ordinate measuring machines (CMMs) that provides an optimal platform for the REVO®...
A-1007-0056 - MCG - comprehensive CMM checking gauge kit (for all CMMs)
Renishaw's Machine Checking Gauge (MCG) provides a simple method of monitoring CMM volumetric accuracy (to ISO 10360-2 standards) at regular intervals between annual service and re-calibration, or...
A-1007-0006 - MCG - small CMM checking gauge kit (for CMMs up to 1 m³)
Renishaw's Machine Checking Gauge (MCG) provides a simple method of monitoring CMM volumetric accuracy (to ISO 10360-2 standards) at regular intervals between annual service and re-calibration, or...
Post-process monitoring
The post-process monitoring layer of the Renishaw process pyramid concerns checking the process and the finished part against their specifications, as well as logging process routes and outcomes.
Apex improves capabilities and responsiveness through investment in 5-axis CMM technology and flexible gauging
A step-change in macro-economic factors led CMM specialists, Apex Metrology Ltd (Apex), to conduct a strategic review of its service offering.
5-axis technology
5-axis technology Based on advanced head, sensor and control technology, Renishaw's 5-axis measurement technology delivers unprecedented measuring speed and flexibility, whilst avoiding the speed...
Retrofit elements and options
Renishaw provides state-of-the-art technology in all aspects of a CMM upgrade, including sensors, controller and metrology software.
Product CAD models
Product CAD models You do not have permission to access this page please contact Renishaw Support on cmm.
R-PC-13450450-12-6 - M6 CMM Aluminium plate, 12.7 mm × 450.0 mm × 450.0 mm
This CMM precision ground aluminium base plate has multiple M6 threaded holes spaced at 12.
R-PC-13300300-12-6 - M6 CMM Aluminium plate, 12.7 mm × 300.0 mm × 300.0 mm
This CMM precision ground aluminium base plate has multiple M6 threaded holes spaced at 12.
R-PC-19600600-12-6 - M6 CMM Aluminium plate, 19.1 mm × 600.0 mm × 600.0 mm
This CMM precision ground aluminium base plate has multiple M6 threaded holes spaced at 12.
Renishaw’s AGILITY® 5-axis CMM advances EDM machine tool manufacture with fast and accurate 100% inspection
The AGILITY® CMM with REVO 5-axis multi-sensor system advances Beijing DMNC-EDM (China) machine tool manufacture with fast and accurate 100% inspection
R-PC-501818-50-20 - 1/4-20 CMM Aluminium plate, 0.5 in × 18.00 in × 18.00 in
This CMM precision ground aluminium base plate has multiple 1/4-20 threaded holes spaced at 0.
"Nothing else comes close to REVO for CMM inspection”
Aerospace sub-contractor ANT Industries carried out a study on its production processes with the aim to make improvements, it was clear that inspection was a major bottleneck.
Connecting the UCC MMI to a CMM
Connecting the UCC MMI to a CMM Switched inputs Air pressure The controller monitors the input and will signal to the software if it goes open circuit or high.
AGILITY® CMMs with 5-axis technology
AGILITY® CMMs provide a complete metrology solution for the shop floor or the metrology laboratory.
MCG systems
MCG systems The probe's stylus slots into the end of what is, in effect, a reference 'ball' bar.
Legacy product CAD models
Legacy product CAD models Links to our legacy CAD models are listed below.
QuickLoad™ rail system
QuickLoad™ rail system, Fast, easy and repeatable set-ups for CMM part inspection with the QuickLoad rail system., ecom_nav