Filtrovat podle
Nalezen výsledek pro CMM
A-3060-0090 - RCP2 change port for REVO® stylus holders
RCP2 is a passive rack port that provides automatic, high speed changing of the RSH range of stylus holders as well as SFS styli.
A-1371-1001 - TCR20 rack for TP20 on the PH20 head (rack only)
The TCR20 probe module changing rack is designed specifically for PH20 and features a tip correct artefact located at the centre of the rack assembly for PH20 metrology optimisation.
A-2237-1409 - FCR25 TC-L3 three port standalone thermally controlled change rack
The FCR25 TC-L3 is a triple port standalone rack, based on the FCR25 TC. It provides unmatched flexibility where rapid automatic changing of SM25 probe modules is required.
A-2098-0933 - SCP600 stylus change port for SP600M and SP600Q
The SCP600 holds SP600 stylus modules for automatic changing, and protects them from airborne contaminants.
CMM fixture set-up showing clamps, cones and standoffs securing a heat exchange part
CMM fixture set-up showing clamps, cones and standoffs securing a heat exchange part
Figure 2: Temperature change of CMM granite bed (3) and encoder scale (2) compared with room air temperature (1)
Figure 2 of App. note: Substrate mastered scale on a CMM
TP200 probe operation
TP200 probe operation The trigger level selection does not affect sensitivity when the probe is in damped mode.
SPA2-2 system components
SPA2-2 system components A number of kits exist which contain the necessary components required to connect the SPA2-2 onto a CMM.
IS1-2 introduction
IS1-2 introduction The IS1-2 interface selector is a fully automatic system for use on coordinate measuring machine (CMM) installations requiring multiple sensor types (e.
SP25M calibration
SP25M calibration NOTE: As the analogue outputs from SP25M are non-linear and non-orthogonal, a third order polymer non-linear calibration method should always be used for optimum accuracy.
RUP1 probe change system
RUP1 probe change system RCP TC-3 The RCP TC-3 is a thermally controlled port for changing RSP3-6, SFP2 and RUP1 probes.
PH20 installation and user's guide
PH20 is a dynamic measuring head and probe system from Renishaw.
PI 7-3
PI 7-3 Special auto-selecting electronics within the interface allow exchange of these probes without any changes to the interface.
PHS-2 installation
PHS-2 installation The PHS-2 probe head mounts onto the CMM quill via a kinematic mounting plate.
Software installation
Software installation Support for the UCC PI 80 is included in UCCsuite version 5.
Additive manufacturing orthopaedic implants for Croom Precision Medical
Reliability and consistency are key attributes to any manufacturing operation but especially so in the orthopaedic implant industry.
Installing the system
Installing the system The rack mount bracket kit is part no.
Customer training on CMM, Renishaw Inc
customer training,renishaw inc on CMM
CMM technology guide front cover image
Image of Renishaw's CMM technology guide
Using machine tool probes for precision metrology in the manufacturing of forged wheel and car chassis
The automotive industry is fiercely competitive.
AGILITY CMM and REVO-2 head with SFP2
AGILITY CMM with the REVO 5-axis multi-sensor system's SFP2 surface finish probe and MCU joystick in situ (close up).
AGILITY CMM with REVO-2 and MRS2 rack
REVO-2 head and REVO 5-axis multi-sensor system's RSP2 scanning probe and MRS2 rack viewed through the holes in the AGILITY CMM.
AGILITY CMM with REVO-2 and MRS2 rack
REVO-2 head and REVO 5-axis multi-sensor system's RSP2 scanning probe and MRS2 rack viewed through the holes in the AGILITY CMM (close up).
REVO on AGILITY CMM on Control stand 2025
Professional stand photography taken at the Control Show 2025 in Germany. REVO on AGILITY CMM on the stand.
Post machining inspection with Renishaw PH10 CMM probe
An image showing post machining inspection with a Renishaw PH10 CMM Probe
Discussions about AGILITY CMM on Control stand 2025
Professional stand photography taken at the Control Show 2025 in Germany. Staff and visitor discussing AGILITY CMM on stand.
REVO on an AGILITY CMM at Control 2025
Professional stand photography taken at the Control Show 2025 in Germany. REVO on an AGILITY CMM on the stand.
AGILITY CMM with REVO-2 and MRS2 rack
REVO-2 head and REVO 5-axis multi-sensor system's RSP2 scanning probe and MRS2 rack viewed through the holes in the AGILITY CMM.
PL107 PHS1 / PHS-2 overtravel cable
This straight cable has a 15-pin high-density D-type socket (NOT supplied) at end 'A' and is supplied unterminated at end 'B', allowing the cable to be threaded through the CMM cable tracks.
Adjustment modules
Adjustment modules AM1 adjustable module The AM1 adjustment module is designed to provide quick and accurate angular alignment of the PH6M and PH10M PLUS with the axes of the CMM and Renishaw ACR3.
MCU (H-1000-5182) - legacy
The manual control units are comprehensive CMM joystick controllers designed for use with Renishaw's universal CMM controller range.
Heavy industry
Manufacturing for the construction, agriculture, rail and heavy plant sectors requires high-quality and reliable large part machining capabilities.
“Gauging time and costs cut by 80% and accuracy maintained despite a 21°C range”
Kishan Auto parts Pvt.
AGILITY CMMs banner
Graphic banner image of an AGILITY CMM.
PH10M-iQ PLUS references and associated documents
PH10M-iQ PLUS references and associated documents It is recommended that the following documentation is referenced when installing and using the PH10M-iQ PLUS: Title Document number User's guide...
BG - Безопасност
BG - Безопасност ПРЕДУПРЕЖДЕНИЕ: SPA3 трябва да се заземи.
NL - Veiligheid
NL - Veiligheid Gebruik van deze apparatuur op een manier die de fabrikant niet voorgeschreven heeft, kan de veiligheid van de apparatuur beperken.
SPA3-2 safety
SPA3-2 safety If the equipment is used in a manner not specified by the manufacturer then the safety of the equipment may be impaired.
EN - Safety
EN - Safety Where this symbol is displayed on the product the user must refer to the installation guide for information and safety advice.
PT - Segurança
PT - Segurança Se o equipamento for utilizado de uma maneira não indicada pelo fabricante, a segurança do equipamento pode ficar comprometida.
EL - Ασφάλεια
EL - Ασφάλεια Εάν ο εξοπλισμός χρησιμοποιείται με τρόπο μη προδιαγεγραμμένο από τον κατασκευαστή, τότε η ασφάλεια του εξοπλισμού πιθανώς να παρεμποδίζεται.
EN - Safety
EN - Safety WARNING: SPA3 is isolated from the power supply by disconnection of the ac power connector from the external PSU.
NL - Veiligheid
NL - Veiligheid Gebruik van deze apparatuur op een manier die de fabrikant niet voorgeschreven heeft, kan de veiligheid van de apparatuur beperken.
SPA3 safety
SPA3 safety WARNING: Maintenance should only be carried out after the machine has been isolated from the electrical supply, compressed air supply or other energy sources in accordance with the...
MCG part program generation
MCG part program generation DMIS sequence generator To generate a part programe please do the following: Select the length of the MCG arm from the 'Arm length' dropdown list: Click on 'Write...
FCR25 TC warm up time
FCR25 TC warm up time When an FCR25 TC is used with SM25 scanning modules, all components must reach the correct operating temperature for optimum metrology performance.
IT - Sicurezza
IT - Sicurezza AVVISO: SPA2-2 deve essere messo a terra.
EL - Ασφάλεια
EL - Ασφάλεια ΠΡΟΕΙΔΟΠΟΙΗΣΗ: Η διακοπή ή απομόνωση του SPA3 ΔΕΝ μπορεί να εμποδίσει μη αναμενόμενη κίνηση του μηχανήματος.
AGILITY CMMs banner
Graphic banner image of a Renishaw AGILITY CMM.