Filter by
Results found for Retrofit Renishaw
FCC (USA only)
FCC (USA only) Information to user (47CFR section 15.
Overtravel unit
Overtravel unit Overtravel unit deflection: The overtravel unit protects the PHS1 probe head in the event of a collision by deflecting and providing an electrical signal which can be used by the...
PH10 Trigger Force Gauge (gram gauge)
PH10 Trigger Force Gauge (gram gauge) NOTE: To convert mass in grams to trigger force in Newtons the following equation is used: Trigger force in Newtons = Mass in grams/100 For example:...
Installation videos for machine tool products
Installation videos for machine tool products A video guide to help you install your Renishaw machine tool probing system.
SFP2 specifications
SFP2 specifications Operating temperature range +10 °C to +40 °C (+50 °F to +104 °F) Storage temperature range -25 °C to +70 °C (-13 °F to +158 °F) Operating humidity 0% to 80% (non-condensing) ...
FCC (USA only)
FCC (USA only) Information to user (47CFR section 15.
Shareholder events
Shareholder events Shareholder events 2025-2026 In line with our commitment to improve investor communications, our Capital Markets Day was held on 17 June 2025, for the financial community,...
Overtravel unit
Overtravel unit The overtravel unit protects the PHS1 probe head in the event of a collision by deflecting and providing an electrical signal which can be used by the CMM controller to stop machine motion.
Manually mounting / removing the stylus from stylus holders
Manually mounting / removing the stylus from stylus holders CAUTION: Failure to use two tools as shown is likely to break the stylus holder.
Automated workpiece set-up boosts forestry equipment manufacture
To meet rising demand for its market-leading range of forestry equipment, Tigercat Industries Inc.
ET - Ohutus
ET - Ohutus ETTEVAATUST! REVO-2 peaosa on valmistatud hõõrdevabade laagritega.
Functional Safety optical encoders
Certain machinery safety functions, such as Safely Limited Speed (SLS), require the encoder feedback to be functionally safe.
Study polymers and microplastics with Raman spectroscopy
Optimise polymer performance. Use Raman spectroscopy to investigate polymers and understand their properties
Identifying particulates and contaminants with Raman spectroscopy
Identifying particulates and contaminants with Raman spectroscopy We're here when you need us To find out more about this application area, or an application that isn't covered here, contact our...
EN - RUP1 Safety
EN - RUP1 Safety RUP1 Remove protective caps prior to use: The RUP1 probe should be handled with care Avoid dropping the RUP1 probe or colliding with workpieces or parts of the CMM structure...
RO - Măsuri de siguranță RUP1
RO - Măsuri de siguranță RUP1 ATENȚIE: Înainte de despachetarea și instalarea sistemului REVO-2 și a palpatoarelor aferente, utilizatorul trebuie să citească cu atenție instrucțiunile de siguranță...
NL - Veiligheid RUP1
NL - Veiligheid RUP1 Hydrophilic polymer elastomer ball De hydrophilic polymer elastomer ball bevat onder meer de volgende bestanddelen:: 60-80% ethaandiol ethyleenglycol 1-3% 2-propeenzuur,...
MCU W-2 legacy hand controller
The wireless manual control unit (MCU W-2) is a comprehensive joystick designed for use with Renishaw's range of UCC controllers
Renishaw’s unique ATOM™ encoder is key to enhanced metrology performance
Renishaw has launched REVO-2, a new improved version of the revolutionary multi-sensor 5-axis measuring head for use on Co-ordinate Measuring Machines (CMMs).
Renishaw’s new VIONiC™ encoder offers unparalleled performance
Renishaw, a world-leading metrology specialist, recently launched the VIONiC™ series, a new family of ultra-high accuracy, super-compact all-in-one digital incremental encoders.
Renishaw’s new VIONiC™ encoder offers unparalleled performance
Renishaw, a world-leading metrology specialist, recently launched the VIONiC™ series, a new family of ultra-high accuracy, super-compact all-in-one digital incremental encoders.
Power Plus - Virtual Reality - The beauty of vision technology with the accuracy and repeatability of Renishaw encoders
Power Plus offers high precision camera positioning for virtual reality technology in the broadcasting industry, with the help of Renishaw’s optical and magnetic encoders to support accuracy and...
Renishaw hosts UK Prime Minister and Chancellor of the Exchequer for visit focused on research and development
The Prime Minister Theresa May and Chancellor of the Exchequer Philip Hammond visited Renishaw’s headquarters site near Wotton-under-Edge in Gloucestershire, yesterday (24th November) for a tour of...
Renishaw balloon flying in the Lord Mayor's Hot Air Balloon Regatta 2015 (image courtesy of Exclusive Ballooning)
London’s skies were filled with hot air balloons on 7th June, as Renishaw’s G-RENI joined around 40 other balloons in the historic Lord Mayor’s Appeal Hot Air Balloon Regatta, raising over £75,000...
UCC MMI introduction
UCC MMI introduction The UCC MMI is an interface for use on manual CMMs to interface and connect encoder and probe signals to the PC.
System requirements
System requirements 100 Vac - 240 Vac -15%, +10% 47 Hz to 63 Hz 750 W maximum Mains input connector IEC C13 10 amp power connector Ensure that a suitable cable is always used that meet the...
System components overview
System components overview System overview The modular design of the SP25M system enables the flexibility for optimum configuration by the user.
SP25M maintenance
SP25M maintenance CAUTION: Always adhere to the general safety recommendations in this document.
References for the PH10
References for the PH10 The following Renishaw documentation is referred to in this document or may be a source of further relevant information, these documents can be downloaded from the...
UCC MMI-2 installation guide
The UCC MMI-2 controller provides a USB based interface for manual CMMs.
Renishaw reduces machining time for aerospace impeller manufacturer
Honeywell Aerospace, part of global commercial and consumer engineering conglomerate Honeywell, produces a large number of the impellers and blisks used in commercial aeroplanes.
Renishaw reduces machining time for aerospace impeller manufacturer
Honeywell Aerospace, part of global commercial and consumer engineering conglomerate Honeywell, produces a large number of the impellers and blisks used in commercial aeroplanes.
TONiC™ FS incremental encoder system with RESM20 rotary (angle) ring
Discover the TONiC™ FS encoder series, Renishaw’s most versatile incremental optical encoder.
VIONiC™ incremental encoder system with RESM20 rotary (angle) ring
Discover the VIONiC™ encoder series, Renishaw’s highest performing incremental optical encoder.
TONiC™ incremental encoder system with RESM20 rotary (angle) ring
Discover the TONiC™ encoder series, Renishaw’s most versatile incremental optical encoder.
Machine tool apps
We are committed to developing a range of machine tool apps for our customers which make installing, configuring, using and maintaining our systems even easier.
New General Manager for Renishaw’s Swedish subsidiary
World leading technology company Renishaw has appointed a leading figure from the Swedish metrology industry to head up its Nordic operations.
Royal interest in Renishaw’s research work
Renishaw’s research facility at Exeter University enjoyed a visit this week from HRH The Princess Royal, who was at the University to officially open Phase II of its Innovation Centre.
Bo Eneholm, New General Manager for Renishaw’s Swedish subsidiary
World leading technology company Renishaw has appointed a leading figure from the Swedish metrology industry to head up its Nordic operations.
Renishaw’s Chairman honoured with international engineering award
Sir David McMurtry, Chairman and Chief Executive of global engineering company Renishaw plc, has been honoured with the prestigious General Pierre Nicolau Award by the International Academy for...
Renishaw’s Head of Sustainability named one of The Manufacturer’s Top 100 manufacturing role models
Ben Goodare, Head of Sustainability at Gloucestershire based global engineering technologies company, Renishaw, has been selected as one of The Manufacturer’s Top 100 role models for the...
Manual probe heads description and operation
Manual probe heads description and operation Renishaw manual probe heads provide the mechanical and electrical connections required when using the majority of Renishaw touch-trigger probes...
Advanced laser tool setters for CNC machines
A range of non-contact laser tool setters and broken tool detection systems for CNC machining centres.
SP80 specification
SP80 specification Probe attributes Ultra-high accuracy scanning probe with three axis measurement (±PX, ±PY, ±PZ)* Orientation Horizontal Size 80 mm × 80 mm (3.
System installation
System installation PH20 initialisation and commissioning sequence The PH20 system should be commissioned using Renishaw's UCCassist-2 software.
UCC AI installation guide
The UCC AI is required for large higher voltage CMM systems which may require motor voltages in excess of 80 V or motor currents in excess of 10 A.
CCD detectors for Raman spectroscopy
CCD detectors for Raman spectroscopy Broadband spectrum of SiC showing photoluminescence (PL) features.
Connectors and signals
Connectors and signals Key Description Key Description 1 Scale 0 interface (15W HDD socket) * 9 UCC - EXP (RJ45 socket) 2 Scale 1 interface (15W HDD socket) * 10 UCC - SPA (RJ45 socket) * 3...
Renconnect use
Renconnect use Renconnect is a powerful support tool that provides a link between you and the resources of the Renishaw CMM support team.
MCU safety
MCU safety CAUTION: Before unpacking and installing the MCU W system, the user should carefully read the safety instructions below and ensure that they are followed at all times by all operators.