Filter by
Results found for “Manual setting and NC programming is needless torture for machine operators…”

Contact tool setters installation videos
Contact tool setters installation videos Below you can find generic videos, as the principles for most tool setter installations are similar, as well as installation videos for TS27R.

UCC DMT introduction
UCC DMT introduction Software setup Error mapping is carried out through UCCassist-2 using the sequence player.

Machine I/O (44W HDD socket)
Machine I/O (44W HDD socket) Enable air solenoid An active low signal to engage an air solenoid.

A-5472-3000 - Primo™ 3D Tool Setter full stylus assembly

Tool setting stylus with a precision ground tip that can be used for setting the tool's length and diameter. It can also act as an artefact for calibrating the Primo Part Setter spindle probe.

Motorised head and autochange rack controllers
A range of control systems to interface between Renishaw's motorised heads and autochange racks and your CMM.

Non-contact tool setter – Using off-centre measurement for oversized tools with NC4
In this tool setting how-to video, Dan and Iain explain how to measure oversized tools using an NC4+ Blue laser tool setter.

MCU fault finding
MCU fault finding Many operating problems can be solved by checking the MCU status LEDs, the system configuration and current operating conditions.

MCU fault finding
MCU fault finding Servos will not engage E-STOP not connected correctly E-STOP still asserted An outer limit switch is activated No screen display Check cable connection NOTE: As with most cable...

Accuracy is everything
Precision engineering for aerospace and automotive sectors demands a proactive approach to complex part verification.

Accessories for the Equator™ comparator system
Accessories for the Equator™ comparator system Button interface - A-6088-0010 The Equator Button Interface allows push button operation of an Equator system.

Post-process monitoring
The post-process monitoring layer of the Renishaw process pyramid concerns checking the process and the finished part against their specifications, as well as logging process routes and outcomes.

MIH introduction
MIH introduction Renishaw's MIH is a compact manual indexable probe head which offers the flexibility and time saving normally associated with direct computer controlled (DCC) machines and motorised...

Usage
Usage Support documents providing advice and assistance on issues which may be encountered when using Productivity+™ applications.

Breakthrough mobile technology relies on Renishaw encoders
A revolutionary mobile phone antenna has been developed by UK company Sarantel, based on the company's patented PowerHelix™ technology.

Testing and verification
Testing and verification NOTE: It is recommended that metrology tests should be performed after any update.

Machine setting checks performed on RAMTIC machining centre
Renishaw RAMTIC with OMP400 probe checking repeatability and alignment for indexer and artefact

Renishaw's new smart manufacturing data platform showcases smart factory automation at IMTS 2024
Renishaw Central is a manufacturing connectivity and data platform that collects and presents manufacturing process data.

EN - Safety
EN - Safety WARNING: Switching off or isolating the SPA3 may NOT prevent unexpected machine movement.

SPA3 safety
SPA3 safety Where this symbol is displayed on the product the user must refer to the installation guide for information and safety advice.

SPA3-2 safety
SPA3-2 safety WARNING: The SPA3-2 must not be powered directly from the mains.

Connecting the UCC controller
Connecting the UCC controller b) Pressing 'Next' will bring up a screen to allow the specific controller to be selected.

Connecting the UCC controller
Connecting the UCC controller c) Click on 'Properties' and select ‘Internet Protocol (TCP/IPv4)' and click 'Properties'.

Connecting the UCC controller
Connecting the UCC controller Hardware connection The host PC must have a dedicated ethernet connection to the UCC controller.

Connecting the UCC controller
Connecting the UCC controller Software installation The UCCassist-2 software must be installed on the host PC prior to connection of the UCC controller.

IS1-2
IS1-2 Extended warranty For peace of mind a 3-year warranty is available for your new CMM products during the first 3 months from purchase.

GoProbe for Primo - Siemens
This manual contains detailed information on the GoProbe for Primo part setting and tool setting cycles for use on Siemens controls.

PLM6 and PLM7 machine cables
These two straight cables each have a 15-pin D-type plug at end 'A' and a 14-pin chassis-mount LEMO socket supplied loose for fitment to end 'B'.

Testing and verification
Testing and verification The manufacturer of the finished machine, or the installer of the UCC MMI, is responsible for ensuring that the following testing and verification, to the appropriate...

A-5003-2287 - M2 Ø6 mm ruby ball, carbon fibre stem, L 50 mm, EWL 50 mm

Straight styli are designed to inspect simple features where direct, unobstructed contact with a measured surface is possible.

White papers - Calibration products
White papers - Calibration products Browse documents Supporting documents Laser diagonal measurement for machine tool performance assessment Ballbar testing with circle, diamond, square machining...

Open optical encoders for motion control
Renishaw provides an extensive range of open optical encoder systems.

Renishaw incremental encoders enhance the stability and efficiency of lens testing
The smartphone has become increasingly ubiquitous in recent years with significant penetration throughout the world.

Jingdiao's refusal to compromise on quality sees its business take off
Beijing Jingdiao Company Ltd has collaborated with Renishaw as its business has continued to grow over the years, with the two companies working together to open up new pathways to innovation and...

PL157 machine cable adaptor for IU80
This straight cable has a 15-pin high-density D-type socket at end ‘A' and an in-line 14-pin LEMO plug at end ‘B'. It is used to electrically connect the SP80 scanning probe to the CMM quill.

A-8003-1304 - Swivel mirror

The swivel mirror allows adjustment to be made along machine diagonals, or on inclined axes.

Renishaw extends its range of AGILITY® 5-axis technology multi-sensor CMMs.
Renishaw, a world-leading manufacturer of engineering and precision measurement systems, now offers a range of co-ordinate measuring machines (CMMs) that provides an optimal platform for the REVO®...

A-6088-0010 - Equator™ Button Interface (EBI)

The Equator Button Interface is designed for shop-floor operators, with simple push-button controls that remove the need for a mouse and keyboard.

Upgrade your system
Renishaw offers existing users a range of options to provide you with the best solution to upgrade to the latest system.

A-1034-0028 - Datum ball kit, Ø12 mm

The Renishaw universal datum sphere enhances the performance of manual and fully automated CMMs.

Equator gauging system leads to 30% increase in manufacturing capacity
Manual gauging processes were incapable of delivering the throughput necessary to achieve a high-volume part-manufacturing target at Olympus NDT.

A-5000-4155 - M2 Ø5 mm ruby ball, stainless steel stem, L 10 mm, EWL 10 mm

Straight styli are designed to inspect simple features where direct, unobstructed contact with a measured surface is possible.

A-2063-6098 - LP2 probe kit

A-2063-6098 LP2 probe kit High-performance, compact probe suitable for inspection and tool setting applications.

A-2064-0002 - LP2H probe kit

A-2064-0002 LP2H probe kit High-performance, compact probe suitable for inspection and tool setting applications.

Machine I/O
Machine I/O +24 Vdc +24 Vdc limited to 1 A.

Manual clock
The old-fashioned way of setting parts - the operator establishes the location of a datum feature by 'clocking' it.

Testing and verification
Testing and verification NOTE: It is strongly recommended that any measuring equipment is regularly checked for accuracy.

ATOM DX™ incremental encoder system with RKLF linear and partial arc scale
ATOM DX™ incremental encoder system with RKLF linear and partial arc scale Easy fault finding and servicing The Advanced Diagnostic Tool acquires comprehensive real-time data from ATOM DX...

First metal 3D printed bicycle frame manufactured by Renishaw for Empire Cycles
Renishaw, the UK’s only manufacturer of a metal-based additive manufacturing machine that prints metal parts, has collaborated with a leading British bicycle design and manufacturing company to...

SP80 safety
SP80 safety There is no overtravel protection in the +Z axis other than an end stop.

SP80 safety
SP80 safety There is no overtravel protection in the +Z axis other than an end stop.