Filter by
Results found for “Manual setting and NC programming is needless torture for machine operators…”

Renishaw XM-60 多光束校正儀大幅提高空間誤差量測效率
在量測空間精度相關誤差時需要考慮諸多因素,而量測所有誤差需要花費很長時間。 For example, there are tracker type volumetric precision measurement systems where, as the size of the machine increases, the measurement time required increases...

Raman spectroscopy for the earth sciences
Raman spectroscopy for the earth sciences Renishaw 以獲獎無數的 inVia 共軛焦拉曼顯微鏡、拉曼/掃描測頭組合顯微鏡系統,以及 SEM 拉曼組合型系統等創新科技,持續努力擴展應用範圍。 按一下以下連結,深入瞭解我們如何協助您的地球科學應用進行: 我們隨時為您服務 若要深入瞭解此應用領域或未涵蓋到的應用,請聯絡應用團隊。 聯絡應用團隊 ...

Raman spectroscopy for the chemical sciences
Raman spectroscopy for the chemical sciences 我們隨時為您服務 若要深入瞭解此應用領域或未涵蓋到的應用,請聯絡應用團隊。 聯絡應用團隊 Renishaw 以獲獎無數的 inVia 共軛焦拉曼顯微鏡、拉曼/掃描測頭組合顯微鏡系統,以及 SEM 拉曼組合型系統等創新科技,持續努力擴展應用範圍。 按一下以下連結,深入瞭解我們如何協助您的化學科學應用...

British Cycling races ahead with Renishaw additive manufacturing
British Cycling is the national governing body in Great Britain for cycling, as recognised by the Union Cycliste Internationale (UCI).

How to optimise your encoder system
Ensure your optical encoder system is optimised to achieve the best performance. This webinar explores external and internal factors that can influence the performance of your encoder.

Digital evolution of cranial surgery
From complex reconstructive facial surgery to orthopaedic and trauma surgery, advances in additive manufacturing have inspired a growing number of progressive surgeons to commission metal 3D printed...

LeanWerks 個案研究
LeanWerks developed a process combining cutting tool, workholding and part-probing technologies to enable its turn-mill to machine five sides of this investment casting part in one setup.

為什麼選擇測頭?
為什麼選擇測頭? 測頭 是精心製造的開關,在接觸時觸發,會在「事件」發生時,也就是接觸物件表面時,具備高度重複觸發特性。 增加自動化操作進而降低人為介入 貴公司經常需要仰賴技術資深的操作員保持機器的正常運作,而導致人工成本及超時加班費用居高不下嗎?或者工程師忙著從事現場支援,完全無餘力開發新製程? 若您能夠將手動設定和量測程序自動化呢? 降低現場支援成本 減少直接的人力成本...

Raman spectroscopy for the life sciences
Raman spectroscopy for the life sciences 按一下以下連結,深入瞭解我們如何協助您的生命科學應用進行: 您可使用這項無需標示的分析技術,在各種生命科學應用取得化學與結構資訊。 生物製程 蛋白質/縮氨酸結構分析 微生物學 試管內與活體內藥物傳遞 癌症研究/病理學 氧化還原生物學 再生醫學 拉曼光譜已成功應用於分析各種人類、動物及植物細胞和組織。 ...

Ferrari additive manufacturing
Ferrari is a legend, the most loved Italian brand in the world, and at the heart of this myth, their racing department, have two Renishaw additive manufacturing (AM) machines.

Automotive transmission supplier Flexible Concepts guarantees process capability with Equator™ gauge
Automotive transmission supplier Flexible Concepts is using innovative engineering coupled with the Renishaw Equator gauge to guarantee its process capabilities and deliver a highly reliable service...

Where information really counts, fibre-optic broadband cables are fed underground with the help of Renishaw’s rugged encoders
With many countries moving to high-speed, fibre-optic broadband, there is a significant challenge to replace the mass of existing underground cables quickly and easily.

Raman service and support
Raman service and support Raman Revealed Raman Revealed 研討會適合新進使用者參加,以協助更充分運用拉曼系統功能。 檢視詳細資料 升級諮詢 我們可以為想要升級儀器的客戶提供建議,推薦最理想的解決方案,因應您持續變動的實驗需求。 升級諮詢 安裝系統 Renishaw 國際服務團隊將安裝及測試您的系統。團隊由專精拉...

如何使用循圓測試儀
如何使用循圓測試儀 資料擷取 「傳統」測試要求機台執行兩個連續圓,一個為順時針方向,一個為逆時針方向。在實務中,測試圓的前面和後面分別添加了一段圓弧,分別用於機台加速和減速。 通過使用延長桿,可以選擇測試半徑,以反映機器的尺寸和對特定問題的敏感度(例如,大圓更適合發現機台幾何誤差,小圓則對伺服不匹配或滯後更敏感)。...

Photoluminescence spectroscopy and fluorescence explained
Renishaw’s spectrometers can perform photoluminescence (PL) spectroscopy to reveal the electronic structure of a material.

Deep Water Imaging
High accuracy magnetic ring encoders made by RLS, a Renishaw associate company, are used by Martech of Dorset in its Pan and Tilt units for positioning subsea sonar-imaging devices.

SP80 和 SP80H
SP80 和 SP80H 延長保固 自購買全新三次元量床產品當日起,您可在 3 個月內選購 3 年保固 服務,免除您的後顧之憂。請聯絡您的供應商。 SP80 是一種採用數位光學尺和讀取頭技術,外加 Renishaw 創新的隔離光學量測原理的軸套安裝式掃描測頭,即使在使用長測針的情況下,依然能提供優異的掃描效能。SP80 能攜帶最長至 1000 mm 長度及 500 g...

Combined Raman systems
Combined Raman systems SPM/AFM:奈米解析度 將 inVia™ 拉曼顯微鏡結合原子力顯微鏡 (AFM) 等掃描測頭顯微鏡 (SPM),可用來研究材料的化學與結構特性。其中以針尖增強拉曼光譜 (TERS) 增添奈米級化學解析度,並揭露機械特性等補充資訊。 檢視詳細資料 您可以用兩種以上的技術分析樣品,無須在兩種儀器之間奔波,進而達到最大效率。利用...

Modulation matters - how to build all features great and small
The feature article details how versatile laser modulation can help to match the mode of energy delivery to the needs of component features of all sizes. Download the article to find out more.

升級任何 CMM
升級任何 CMM 充分發揮您 CMM 的潛能 請閱讀這份白皮書,瞭解如何透過先進科技軟體、控制器和感測器技術的改裝,為您帶來提升量測能力與現有 CMM 效能的契機。 5 軸量測系統 透過改裝,CMM 所有品牌的使用者都能享有 Renishaw 5 軸量測系統 REVO® 與 PH20™ 的高效能。與傳統 CMM 量測方法不同的是,5 軸量測技術使用同步化的 CMM...

改裝 CMM 提升量測速度
改裝 CMM 提升量測速度 延長保固 自購買全新三次元量床產品當日起,您可在 3 個月內選購 3 年保固 服務,免除您的後顧之憂。請聯絡您的供應商。 MeasureMax* 使用者 MMclient 為可讓現有 MeasureMax 程式,在採用 Renishaw UCC 控制器系統的 CMM 上執行的軟體產品。 * MeasureMax 為 Hexagon Metrology Inc.

工具機應用程式
我們致力開發各種工具機應用程式,以利客戶更容易安裝、設定、使用並維護我們的系統。智慧型手機應用程式提供簡易便捷的方式,使用者只要動動手指就能取得資訊。我們免費的應用程式提供全球各種語言版本,最適合新手或經驗不足的使用者。機上應用程式可完美整合廣泛品牌的 CNC 控制器。

Blog post: A 3D printed mountain bike that you can buy today!
Demand for high specification bicycles has exploded in recent years as both professionals and 'prosumers' have sought a performance edge.

Renishaw on high with Airbus A380 Superjumbo
Airbus A380 aeroplane utilises linear encoders on wing-panel assembly machine

Optical encoders and LiDAR scanning
Optical encoders and LiDAR scanning 光達的運作方式? 光學雷達是一種光學遙感技術,可向目標物體發射雷射光束 (通常為脈衝雷射)。自從十年前 Google 地圖的街景攝影車開始在路上掃街攝影,現在我們對於類似的雷射掃描設備多已見怪不怪。 標準的光達掃描系統是由一個具有旋轉掃描鏡的雷射測距儀與各種定位和定向系統 (POS) 所組成,包括...

Renishaw自動化工業大展強力出擊,用「智」動化精密量測解決方案提升製造效率
2018 年7月18 日 -- 2018台北國際自動化工業大展即將開展,全球精密量測領導廠商 Renishaw 將於8月1日至8月4日於台北南港展覽館4樓 N1028 攤位帶來精準的運動控制方案以及多項精密量測解決方案,透過智慧製造的方式,幫助廣大製造業者們更進一步體驗到自動化帶來的龐大效益。

Thank you for signing up to our newsletter
Thank you for signing up to our newsletter Hero text for newsletter thank you page 影片 歡迎造訪我們的 YouTube 播放清單觀看各種產品示範,以及拉曼光譜的應用範例。 檢視詳細資料 網路研討會 本公司遍佈全球的應用科學家團隊將提供寶貴見解。可即時或隨需觀看簡報,瞭解本公司產品及各種應用領域。 檢視詳...

Small wonder impresses Red Bull F1
“A machine left running unmanned with a broken tool would be disastrous…”

Case study: Quality control of diamond-like carbon
New Plasma Technologies (NPT), based in Moscow, Russia, uses a Renishaw inVia confocal Raman microscope for investigating the structure and chemical properties of materials, non-destructively.

數據驅動製造
數據驅動製造 Web browser views allow live data to be displayed, sorted, filtered and plotted.

Flexible consistent inspection at Porsche part supplier
Flexible consistent inspection at Porsche part supplier.

CNC 機上量測應用程式:在 Windows® 平板電腦上安裝
本影片示範如何將 Renishaw 機上量測應用程式安裝到Windows 平板電腦並透過網路線連接到機台上,以及如何配置網路和APP設定。

InfiniAM Central
InfiniAM Central 積層製造系統的遠端製程監控 生產力 生產力頁面顯示各個 AM 系統的使用時間,並顯示執行、停止及冷卻時間。這樣可讓有意瞭解整體設備效率 (OEE) 的使用者,掌握有哪些地方可以提升製造效率。 主要優點 透過智慧型手機應用程式取得行動通知 安全 管理員頁面可讓管理員管理所有使用者權限。系統可透過輕量型目錄存取通訊協定 (LDAP)...

可將風險降至最低的專業方法
可將風險降至最低的專業方法 由 Renishaw 及其認證改裝商提供 效能保證 第一步是嚴格的機器調查,旨在評估每部 CMM 的機械與電子元件。配合 Renishaw 對於所有品牌 CMM 的豐富經驗,能達成高水準的 Renishaw 系統效能。在您許下任何承諾之前,能精準掌握升級後的 CMM 所能帶來的效果。 經認證的校正 Renishaw 已由 UKAS 認證符合 ISO...

Business Partner Code of Conduct
Renishaw's Code of Conduct sets out our expectations of ethical business conduct for all employees in the Renishaw Group.

Analyse gems with Raman and photoluminescence spectroscopy
Analyse gems with Raman and photoluminescence spectroscopy Renishaw inVia 共軛焦拉曼顯微鏡是全球許多寶石學實驗室的首選儀器。 我們隨時為您服務 若要深入瞭解此應用領域或未涵蓋到的應用,請聯絡應用團隊。 聯絡應用團隊 調查包裏體 輕易判斷包裏體的成分,並透過 StreamHR™ 快速共軛焦體積成像顯示其 3D...

Choosing a Raman spectrometer
Watch our three-part webinar series to learn about selecting a Raman system. Renishaw’s Raman spectrometers are packed with patented technologies for excellent performance and ease-of-use.

FORTiS™ 封閉絕對式光學尺下載
FORTiS™ 封閉絕對式光學尺下載 現在就聯繫我們的銷售團隊 請與 Renishaw 聯絡以取得更多資訊及與專家交流。 歡迎探索我們一系列電感型、開放式、封閉式、磁性和雷射光學尺 ,滿足您的工業自動化需求。 下載以下關於 FORTiS 封閉式光學尺系列的技術文件、媒體與個案研究。 技術繪圖 規格資料表 安裝指南 使用者指南 FORTiS-S 光學尺 FORTiS-N...

Additives in Formula 1: technology of the future
Metal additive manufacturing is quickly becoming the technology of the future, but few people know the full extent of the opportunities it offers or the nature of the partnership - in this industry -...

機上掃描 — 工具機性能檢查
使用搭載 SPRINT™ 技術的 Renishaw OSP60 掃描測頭,可藉由 Productivity+™ On-Machine Health Check 循環快速檢查工具機的線性和運動誤差。

Equality in the workplace
At Renishaw, we believe that equality and fairness are critical to the success of our organisation.

Particle Analysis software module for morphologically directed analysis
Particle Analysis software module for morphologically directed analysis 粒子分析軟體模組可識別顯微鏡影像的粒子。其中可報告形態學參數(例如大小和長寬比),然後引導 inVia™ 拉曼顯微鏡依據化學性質加以識別。 需要關注的目標粒子 樣品的拉曼成像可能產生大量粒子,需要長時間進行處理。如果使用粒子分析軟體,就能針對影像...

Responding to production pressure with conformal cooling
Injection moulding allows plastic products to be produced in complex and intricate detail, often in sizeable production runs, with repeatable tolerances and high surface quality.

IS1-2
Renishaw's range of interfaces makes it easy to connect your probe to your machine controller.

Identifying particulates and contaminants with Raman spectroscopy
Identifying particulates and contaminants with Raman spectroscopy 汙染物拉曼分析 拉曼光譜是識別汙染物並協助判斷其來源的實用技術。Renishaw 拉曼系統 提供您最詳實資料,協助迅速輕易識別汙染物。特色: 高靈敏度,具備小於微米的空間解析度 – 分析材料和薄膜的最小細節 拉曼光譜資料庫 – 方便快速識別汙染物 多重雷射...

Renishaw 封閉式光學尺在新型增減材複合工具機上大顯神通
Effective CNC 團隊設計並打造了一款「一體式」工具機,可交替進行積層和減材加工操作。為了協助 Effective CNC 設計和打造新型工具機,Renishaw 派出多個專業技術團隊,在光學尺系統、工具機專用測頭量測系統和刀具設計系統方面提供全方位支援。