Filter by
Results found for Specifications and downloads

Série de encoders ópticos incrementais QUANTiC™
A série QUANTiC representa o conjunto de encoders ópticos abertos incrementais da Renishaw com opções de saída digital ou analógica, metrologia robusta, medição em alta velocidade e fácil instalação...

Série de encoders ópticos incrementais ATOM DX™
A série de encoders ATOM DX é o menor encoder óptico incremental da Renishaw, com saída digital direta do cabeçote de leitura, proporcionando feedback posicional, interpolação onboard e óptica de...

Classifying Brain Tumours with Raman Spectroscopy
Raman spectroscopy can provide surgeons with a wealth of information which could support them in deciding on the most appropriate intervention strategies.

Floating steel encoder scales for SMT
This application note discusses surface mount technology (SMT) applications and presents an example of where linear steel scale (installed to be thermally independent of its mounting substrate) may...

Renishaw’s RESOLUTE™ absolute encoder supports ITRI breakthrough in multi-axis rotary table design
Taiwan's Industrial Technology Research Institute (ITRI ) has addressed the multi-axial machine tool technology trend by developing an advanced dual-axis rotary table, with integrated Renishaw...

Laser encoders an enabling technology for accurate machining of 40 m composite parts
Flow International Corporation has selected Renishaw HS10 and HS20 laser encoders for use on the company's Composites Machining Center (CMC).

Taking precision to new heights - air bearing stages with Renishaw optical encoders
TOYO Nano System Corporation has developed motion stages with a coplanar, patented machine design that use Renishaw’s high-precision optical encoders for position feedback.

Laser encoder improves accuracy of optical connector measurement
Integration of the Renishaw RLE10 laser encoder has enhanced machine alignment, installation and system stability.

Metal additive manufacturing for UAV engine design optimisation
Renishaw, worked with engine manufacturing company Cobra Aero to optimise its design processes for aircraft and motorcycle engines.

EasyProbe
O software EasyProbe para centros de usinagem possibilita preparação fácil e rápida do trabalho e rotinas de medição, podendo ser utilizado por operadores com pouca experiência.

Software de inspeção para centros de usinagem
Software com macros de inspeção para apalpadores Renishaw de preparação e inspeção de peças para centros de usinagem e torneamento.

Custom Raman solutions
Custom Raman solutions Need something different? Range of custom solutions Experience Contacting the Special Products Team Necessita algo diferente? Se os nossos produtos padrão não atendem...

Meios auxiliares
Uma lista de itens auxiliares para complementar os sistemas de manufatura aditiva da série RenAM 500 da Renishaw

MH20i
O MH20i é um cabeçote de apalpador indexável manual, compatível com a série de módulos de apalpador TP20.

Strain-gauge machine-tool probe is right for 5-axis aerospace parts
Flat surfaces and straight lines are rare among the parts produced at Triumph Fabrications in Shelbyville, Indiana, which is a key reason the company upgraded the machine tool probe on one of its...

Making time for Holthinrichs Watches
Michiel Holthinrichs, the founder of Holthinrichs Watches, is working with a Renishaw Additive Manufacturing Solutions Centre to build up his knowledge about the potential of metal additive manufac...

Making time for Holthinrichs Watches
Michiel Holthinrichs, the founder of Holthinrichs Watches, is working with a Renishaw Additive Manufacturing Solutions Centre to build up his knowledge about the potential of metal additive...

Formulário Primo™ Total Protect
Formulário Primo™ Total Protect Links Primo™ úteis Introdução ao sistema Primo O que está incluído no sistema Primo? Primo para preparação automatizada Registre-se para o Primo Total Protect.

Pontas de precisão para metrologia
Descubra como nossas pontas de precisão para apalpadores por contato são vitais na tecnologia de medição industrial e como a Renishaw pode ajudá-lo.

Série de encoders ópticos incrementais VIONiC™
A série de encoders VIONiC™ é o encoder óptico aberto incremental de mais alto desempenho da Renishaw.

Série de encoders ópticos incrementais TONiC™
O encoder incremental óptico TONiC foi projetado para sistemas de movimento de precisão altamente dinâmicos.

SP80 e SP80H
Apalpador de escaneamento montado em coluna SP80 apropriado para utilização com pontas longas e pesadas

Atualização (retrofit) de CMMs para medições mais rápidas
Transforme sua CMM existente através de uma solução de atualização (retrofit), fornecida e suportada pela Renishaw.

Atualize qualquer CMM
Uma atualização (retrofit) Renishaw está disponível para qualquer marca de CMM, inclusive máquinas da Hexagon e Zeiss.

Encoders ópticos de arco parcial
Rotações menores que uma volta completa são medidas com um encoder de arco parcial.

Encoders ópticos rotativos
O controle preciso da posição angular e do movimento rotativo é obtido usando feedback de posição de encoders ópticos rotativos, também conhecidos como encoders angulares.

Equator gauging system leads to 30% increase in manufacturing capacity
Manual gauging processes were incapable of delivering the throughput necessary to achieve a high-volume part-manufacturing target at Olympus NDT.

Productivity+™ – Software de apalpador baseado em PC para centros de usinagem
Software de apalpador baseado em PC para centros de usinagem, que possibilita o controle de processos sofisticados e usinagem adaptativa.

Apalpador para preset de ferramentas por contato TS27R
Apalpador para preset de ferramentas por contato TS27R Links para máquinas-ferramenta Produtos para máquinas-ferramenta Melhore seu processo de produção Qual produto é mais apropriado para as suas...

Precision position feedback for smart manufacturing
As the world enters a new era of smart manufacturing, industry demand for precision motion control systems is increasing to unprecedented levels.

Renishaw calibration systems essential as ‘déjà vu’ hits rebuild specialist Murrall & Lang
In 1989, Leeds-based Dana Spicer needed a large, heavy duty CNC machining centre, to mill, drill, and bore the ends of 2-metre long axle beams, for heavy off-road vehicles.

A tecnologia de fundição a vácuo facilita ciclos de desenvolvimento em tempo recorde para o fabricante de espremedor automático de suco Zumex
A Zumex recentemente investiu em uma máquina de fundição a vácuo 5/01 PLC da Renishaw, a qual possibilitou acelerar o seu ciclo de desenvolvimento e reduzir os custos com terceiros.

The accuracy of rotary encoders
This white paper outlines the major factors affecting rotary (angle) encoder performance to help designers choose the best encoder system for their chosen application.

Raman spectroscopy confirms an ocean's worth of water in the Earth's lower mantle
In recent years, Renishaw’s Raman microscopes located at two prestigious geological institutions have been used for the non-destructive analysis of inclusions in “ultradeep” diamonds from the lower...

Flora Digital prints with Renishaw's optical encoders
Flora Digital, a brand name of Shenzhen Runtianzhi Digital Equipment Co Ltd (SRDEC), specialises in wide-format inkjet technology for the commercial print industry.

Material innovation through metal additive manufacturing
Uniform Wares partnered with Betatype to explore the advantages of additive manufacturing (AM) technology, pushing the boundaries of design in an industry traditionally centred around heritage.

Exchanging metal 3D printing solutions with HiETA
Technology from Renishaw is helping HiETA to move metal additive manufacturing (AM) from prototype manufacture into commercial production of its specialist range of heat exchangers.

Enhancing the additive manufacturing process chain
The design freedom provided by additive manufacturing (AM) or ‘3D printing’ technology is an important enabler in cutting-edge product innovation.

Software poderoso e fácil de usar para apalpadores de máquinas-ferramenta
Os mais recentes softwares baseados em PC para máquinas-ferramenta da Renishaw.

Ambiente configurável
O MODUS possui uma interface Windows configurável pelo usuário, que pode ser alterada de acordo com suas necessidades.

Preset de ferramentas sem contato NCPCB
Preset de ferramentas sem contato NCPCB Solução flexível com preset de ferramentas.

Software de preset de ferramentas
Software de preset de ferramentas Software para máquinas-ferramenta Software de inspeção Software de preset de ferramentas GoProbe Productivity+™ GUIs Renishaw Set and Inspect Reporter...

Qualidade e conformidade dos leitores laser
Quando você compra um sistema de leitor laser Renishaw, você está comprando confiabilidade comprovada e qualidade assegurada.

Comandos
A família de comandos universais UCC para CMMs proporciona controle de movimentos e integração total de sensores Renishaw atuais e futuros.

Serviço dedicado de assistência e apoio ao cliente
Serviço dedicado de assistência e apoio ao cliente O serviço da Renishaw não termina com a conclusão da instalação do produto.

Optimising the design of direct drive valves through metal AM
Domin collaborated with Renishaw to develop a new, stable, state-of-the-art technology suite for the fluid power sector.

Investigating the secrets of Stonehenge with Raman spectroscopy
Renishaw had the privilege to assist in analysing the Altar Stone in situ using a Renishaw Virsa™ Raman analyser.

Introducing the RESOLUTE™ FS encoder
RESOLUTE FS (Functional Safety) encoder systems offer customers the outstanding metrology performance of the RESOLUTE series but with the added peace-of-mind that comes from compliance with the...

Benefícios do controle de processo
Benefícios do controle de processo O uso inteligente das tecnologias de controle de processo na produção tem efeitos benéficos muito além dos aspectos tradicionais de qualidade assegurada dimensional .